This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-050047: Registers reset

Part Number: TIDA-050047
Other Parts Discussed in Thread: TPS25751

Hello,

Working with the TIDA-050047 in a 3S configuration, in a sink-only mode.

Every time after I either plug, or unplug the wall-adapter, I notice that the registers of the TPS25751D are reset.

Is this a normal behavior?

Is there a way around it?

 

Regards,

Yoav

  • Hi Yoav, 

    The TPS25751 registers will reset when the device is power cycled. The TPS25751 can be powered from VBUS (i.e. from wall adapter) or from VIN3V3 (see description from datasheet below). 

    In the reference design, VIN3V3 is generated from the SYS rail on the battery charger. 

    Best Regards, 

    Aya Khedr