This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN3413: What is the difference between TCAN3413 and TCAN3403?

Part Number: TCAN3413
Other Parts Discussed in Thread: TCAN3403, , TCAN3403-Q1

What is the difference between TCAN3413 and TCAN3403?

I am specifically looking for one part to be our main part and another part that can be a drop in replacement. 

Our needs are:  

  • SOIC-8
  • Vcc 3.3V
  • Vio capable from 1.7V to 5.5V
  • Automotive not necessary but could have as an alternate
  • -40C to 85C (or better)
  • supports CAN FD
  • Half duplex