This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX232: Looking for an isolated RS-232 Transreceiver solution

Part Number: MAX232
Other Parts Discussed in Thread: ISO6441, ISOW6441, ISO6421, TRS3253E-EP

We are looking for an isolated RS-232 transceiver solution with the following specifications:

  • Data Rate: 1 Mbps
  • Isolation: Required (isolated RS-232 transceiver)
  • Operating Temperature Range: -25°C to +105°C or higher
  • Package Type: Any SMD package acceptable, excluding BGA

Please share suitable part numbers, datasheets, availability, and any relevant technical details for evaluation.