Part Number: DS250DF230
Hi,
When adapt mode is set to 2, and register 0x2F[1] is at the default value of 0, is there a way to tell if the CTLE gain used is 0.6dB or 9.2dB from some other register?
From the diagram below, it looks like that these two CTLE boost values have the same read back register value:
The way I'm currently handling this ambiguity is:
- manually record DFE tap values
- set DFE to recorded values and set CTLE to 0.6dB
- get FOM from eye (if recovered)
- set DFE to recorded values and set CTLE to 9.2dB
- get FOM from eye (if recovered)
- compare the two FOM from the two CTLE settings
Which ever FOM is better, then the equivalent CTLE setting can be determined.
This method is quite tedious and time consuming if you have multiple channels.
Are there easier ways to do this?
Regards,
Liang