This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDP0604: Question about TDP0604IRNQT

Part Number: TDP0604

Hello:

At the moment, after adding this TDP0604IRNQT component to the customer's circuit, the entire input signal is not working. Can you help check if there are any problems with the schematic and PCB? The PCB picture is a cropped image, thanks!!!

TDP0604IRNQT.pdf PCB_TDP0604IRNQT.zip 

  • Hi Jimmy,

    Members of our team are out of office this week, so I will need time to review these files. Please allow me until Thursday or sooner to provide feedback.

    Best,

    Shane

  • Jimmy

    Looking at the schematic, you have 20k pulldown on MODE pin. This will disable the DDC buffer, but it looks like you are using the DDC buffer in this design. In this case, you should change MODE pin to 1k pulldown.

    With 1k pulldown on MODE pin, please make sure both CFG0 and CFG1 have 1k pulldown to GND as well. 

    The EN pin has an internal 250k pull-up to VIO, so you should remove the external pullup resistor and have an external pulldown capacitor to create a passive reset circuit. 

    Any chance you can probe the DDC bus first after making these changes?

    Thanks

    David