Part Number: TCA4307
Hi,
I'm facing an issue where hot-plugging a board into a live backplane causes damage to one or more TCA4307 devices located on the daugther cards.
Our design is a backplane with multiple daughter cards that are all hot-swappable. Each daughter card includes a TCA4307 device to protect their SCL/SDA lines that connect to the global I2C interface on the backplane. The daugther cards have staggered connector with ground-first contact.
The backplane also includes a separate 10-pin header that is used to connect a small control module. The connector for that module is a simple wire-to-board header, without staggered pins. The PCB of the module is at the other end of a 100mm AWG22 wire harness. That control module also includes a TCA4307 device and also connects to the backplane's global I2C interface.
When I do a hot insertion of the control module into the live backplane, it will frequently damage one or more of the TCA4307 devices located on the module itself and/or on the daughter card. A damaged device will hold the SDA and/or SCL line permanently low or have an intermediate voltage, resulting in a pernanently stuck interface for the entire system. We need to replace the broken TCA4307 devices to make the I2C interface functional again. No other devices are getting damaged in the system.
I was suspecting that the lack of staggered connection on the module could be the source of the issue, therefore I have tried attaching the ground of the control board to the ground of the backplane with a separate wire prior to system power-up, to ensure that the control board and the backplane were at the same potential throughout the experiment. Yet, the devices still got damaged after a hot insertion of the module into the backplane.
The TCA4307 devices all have their VCC pin powered from a unique 3.0V rail from the backplane. The card-sides are powered at 3.3V from on-board regulators. The shared SDAIN/SCLIN lines have 10K pull-up resistors to 3.0V on the backplane, and each daughter card/module has 10K pull-up resistors to local 3.3V on their SDAOUT/SCLOUT pins.
I have looked at the TI application notes and found some discussions about the possibility of stucking the bus during hot-plug, but did not see anything about a risk of damaging the devices. In my mind, the TCA4307 device is by itself the protection and should not die so easily.
Can you please advise on that issue? Can you think of a reason why the TCA4307 are dying and what could be done to protect them?
Note that although our backplane supports multiple daughter cards, at the moment I only have one daugter card and one control module in the system. We have limited supply of proto daugther cards, therefore I don't know yet if hot-plugging a second daugther causes similar problem.
Thanks,
Yannick.