SN65DSI83: SN65DSI83TPAPRQ1- VCORE Value

Part Number: SN65DSI83

Hi Team,

For SN65DSI83TPAPRQ1, I need the VCORE minimum and maximum voltage values for analysis. I am unable to locate these values in the datasheet.

  • Hi Jishna,

    The VCore pin is an output of internal voltage regular that should be 1.1 V nominal. The datasheet does not share a min and max value for it, since it is only meant to be check the voltage level if needed and to 1 uF external capacitor to ground. 

    Is there any particular reason or debug issue for this query? Please let us know if there is an issue or if the pin is not reading approximately 1.1V nominal under normal operating conditions.

    Best regards,
    Ikram