Part Number: TCA9544A
Other Parts Discussed in Thread: TCA9546A, TCA9543A
Hi,
We are evaluating the TCA9544APWR for a multi-channel I²C architecture.
The host controller is connected to the upstream I²C interface of the TCA9544A. The downstream side consists of four independent channels, with each channel connected to one camera via its I²C control interface.
Our main requirement is to control all four camera I²C channels simultaneously, particularly for synchronized control of the cameras' motorized lenses.
Could you please clarify:
Can all four TCA9544A channels be enabled simultaneously?
If all four channels are enabled, can the host transmit the same I²C command to all four cameras simultaneously (broadcast)?
If simultaneous transmission is not supported, what is the minimum practical delay between the same command being sent to the four cameras?
Is there any recommended configuration or method using the TCA9544A to achieve the closest possible synchronization across all four camera I²C channels?
Regards,
Nitheesh