This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1462-Q1: CAN interface issue:- Differential signal Recessive mode failure

Part Number: TCAN1462-Q1

Issue:- Differential signal Recessive mode failure

Observing failures for signal parameters :

  1. Differential_MAX_REC. 
    Expected: -120mV to 12mV 
    measured: 204mV to 300mV



can you please guide on the fix for this ?

  • Hi Pankaj,

    The bus seems heavily loaded.

    Hence, please change your scope from the shown 50 ohm impedance to high impedance and re-verify after ensuring the bus is properly terminated similarly to the CAN standard, thanks.

    Best Regards,

    Michael.