This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1002A: TUSB1002A Redriver addition into the De-embedding section

Part Number: TUSB1002A

Hello,

I want to add TUSB1002A Re-driver IC into the De-embedding section.

I have below questions:

  1. As its active device so can I add it in the De-embedding section ?
  2. Is it fruitful to add it into the De-embedding section ?

 

Regards,

Mahammadirfan