This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP5150AM1: TVP5150AM1IPBSR Pixel Statistics

Part Number: TVP5150AM1

Hi, Im curious to know if there is a way to get essentially a pixel value histogram from the TVP5150AM1IPBSR over the I2C interface? Or pixel statistics in general?

  • Hello Jake, 

    This device no longer has any design support from TI as indicated on the product folder so support is limited to what is currently available on existing documentation. 

    I did a quick check and it does not appear that there is any way to determine histogram, average luminance, min/max pixel value, or similar statistics registers. I2C on this      device is purely a control/configuration interface.

    Status Register #1 Peak white detect (bit 7 of 0x88) is the closest thing to a pixel measurement - it tells you if maximum luma (white) was detected in the active video area, but it's a 1-bit flag, not a statistic.

    If you need pixel statistics, they would have to be gathered downstream - either by reading the 8-bit parallel YUV video output with a frame buffer + CPU/FPGA, or by using a video capture device with a built-in ISP that supports histograms.

    Thanks,

    Chris