Part Number: TCAN3414
Hello
I have a WUP issue on the TCAN3414DR. The transceiver is set into standby, waiting for a WUP pattern. While I am sending a CAN message to the TCAN3414DR, after each dominant a small negative glitch of around 170ns happens on the RXD pin. When the TCAN3414DR has detected a CAN message as a WUP, a 1us negative pulse on the RXD can be seen which is OK. But why are there glitches?
The CAN bus runs at 1MBit. Two devices are on the CAN bus, both have a 240ohm termination resistor. One device is just sending and the other is only listening. The setup is only for testing the TCAN3414DR. On the RXD pin there is nothing connected.
Blue = CANH, Yellow = CAN-L, Green = RXD