Other Parts Discussed in Thread: TUSB1310, TUSB1310A
Hi,
I have a board with a TUSB1310 USB 3.0 Transreciver. The board has a Xilinx Spartan6 board in which i have downloaded our Usb 3.0 Core. I have connected all the pins according the board specification. However I have deduced from that the PCLK from the Phy is not received by our USB 3.0 Core and hence nothing is working as of now.
Is there any special requirement for the TI phy from the USB3.0 Pipe interface other than the standard PIPE interface signal.
Have tried to debug the cause and have come to the coclusion that Phy clk is not received. After going through the user manual I have found 2 signals which are out of my understanding.
1. RESETN
2. OUT ENABLE.
Kindly describe how these signals will affect the O/P of PHY Clk...
Is it necesary on the part of the USB 3.0 Link layer to drive this signals to actually get a valid PHY clKT
Thank You