This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS250DF230: CALIBRATION CLOCK

Part Number: DS250DF230

Hi all,

I have a question about the CALIBRATION CLOCK.
Table 8-6 of the datasheet, the Rate/Sub-Rate Table, states that it is only effective when the calibration clock is 30.72MHz.
When using a 25MHz calibration clock, which registers should I change? Are there any recommended values ​​in that case?

The input rates I want to use are as follows:
25.78125 Gbps
10.3125 Gbps
24.33024 Gbps
10.1376 Gbps

Thanks and regards,
Toshi