This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS250DF230: DS250DF230 SIGCONE GUI

Part Number: DS250DF230

Hi,

I've asked at the web. for access to the device DS250DF230 technical files for having the device's model to load it at the sigcone GUI. my request is pending since 19.5.2025. could you help ?

  • Hi Lior,

    I see your request was approved today.  Can you check if you have access now?

    Thanks,

    Drew

  • Yep, I've received access.

    Under the download link, there is a profile file for the DS250DF230 in SigCon Architect, but the device module ID shown is DS250DF210 instead of DS250DF230.Since the two devices have some different register values addresses, can the same profile file still be used for both devices? 

    Could such a difference cause the DS250DF230 device to fail to load properly from the EEPROM using the HEX file generated by the above SigCon?

    in fact, this is what actually happened, the device modified several register values by itself after boot. can it relate that the module ID does not support all the DS250DF230 registers? 

    Ask
    Explain

    2 Sources