Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS1: S/O: 583502

Part Number: SN65LVDS1

Hello,

 

I have a customer who ordered pn : SN65LVDS1DBVT

qty. 120

 

Per customer: We have an issue with a mixed part on a reel received.
Bad LOT

IS: the label on the tape and reel is marked as 503731-2P1 (U9), but the part inside the tape and reel is marked as "LU18," which corresponds to VR6 (either 503813-1P1 as an alternate or 701245-1P1PB as the primary).

SHOULD BE: the marking and the actual part are matched.

 

Can you verify if this information is correct or they recieved the wrong part?

  • Hi Alexis,

    A part marking of LU18 is not consistent with the SN65LKVDS1DBVT. I am not certain what is meant by VR6, is this a customer designator from their design, and is that how they associating it with the 503813-1P1 and 701245-1P1PB? 

    Do they have a image of the devices in question with the LU18 part marking, I'd be interested to see if this was even the right package.

    Best Regards,
    Brandon Fisher

  • Here are the images, if the reel packaging with information is needed, I can also include. 

    Please advise. Thanks!

  • Hi Alexis,

    In the SOT-23 pictured the correct marking is expected to be SAAI. To clarify, there are closeups for 3 devices here, are they from 3 different reels, 2 different reels or the same reel?

    If you can share the reel packaging information that would be useful as well. Ideally I would like to know which reel corresponds to which device marking you have there. 

    Best Regards,
    Brandon Fisher

  • Hello Brandon,

    Per the customer: ALL PARTS ARE FROM THE SAME REEL

    Thanks

  • Hi Alexis,

    Its difficult to know for certain without direct testing, but based on the information you've shared on the top markings I would say these do appear to be the incorrect parts.

    I would recommend your customer contact their TI Sales representative, and that you proceed in your process for a return if they are requesting one. 

    Best Regards,
    Brandon Fisher