TCAN1145-Q1: Unintended flag asserted

Part Number: TCAN1145-Q1

Hi team,

I'm BCCing my customer.

They observed that FSM_CONFIG[3:1] is set as 010b which is reserved settings. They found it with following handling.

a. Read FSM_CONFIG=>0x00h

b. Power down ECU with following order

        VIO->VCC->VSUP

c. Power up ECU(at this moment, VSUP is around 4V due to residual voltage)

d. Read FSM_CONFIG=>0x04h

Q1. What condition can cause this register setting?

Q2. Is FS_STAT=010b okay to operate the device?

Q3. If Q2 answer is NO, how should user manage this?

Best Regards,

Shoji