Part Number: DP83822HF
Other Parts Discussed in Thread: DP83822IF, DP83822EVM, , TMS320F28388S, MSP430F5529
Hello,
I am currently designing an EtherCAT interface using the DP83822IF and 100BASE-FX, and I am referring to the DP83822EVM schematic and layout as a reference for my circuit design.
I have two questions regarding the 100BASE-FX interface.
1. PHY used on the DP83822EVM
According to the DP83822EVM documentation, the EVM supports 100BASE-FX.
However, when I checked the schematic/BOM, the PHY part number appears to be different from the Fiber-supporting variants of the DP83822.
Could you please clarify:
- Which exact PHY part number is actually mounted on the current DP83822EVM?
- Is the PHY mounted on the EVM capable of supporting 100BASE-FX?
- If the part number shown in the schematic/BOM differs from the actual mounted device, which device should be considered the reference for 100BASE-FX operation?
2. AC coupling capacitors between the PHY and SFP
In the DP83822IF datasheet, AC coupling capacitors are shown on the TX/RX differential signal lines for the 100BASE-FX interface.
However, I do not see these capacitors between the PHY and the SFP connector in the DP83822EVM schematic.
Is my understanding correct that these capacitors are not required on the EVM side because the SFP module used for the EVM already has the AC coupling capacitors internally?
For my EtherCAT design, if the selected SFP module has internal AC coupling capacitors, is it correct that additional AC coupling capacitors do not need to be placed between the DP83822IF and the SFP connector?
If this depends on the SFP module, could you please let me know which SFP specification or documentation should be checked to determine whether the AC coupling capacitors are internally included?
Thank you for your support.