TL16C2550: Behavior Inconsistent with the Datasheet

Part Number: TL16C2550
Other Parts Discussed in Thread: TL16C550D, TL16C752D

Dear Technical Support Team,

While debugging the TL16C2550IPFB, we observed a phenomenon that appears to be inconsistent with the data sheet.

[Observed Phenomenon]

A. Undefined values are read from the IIR

When reading the IIR (Interrupt Identification Register) to check for interrupt causes, values such as “0xC3” and “0xC5”—

which cannot be interpreted as normal IIR values according to the data sheet—are output at a low frequency.

This tends to occur when the INT state change and the IIR read timing are close together.

We have since modified the process to read the IIR only after confirming that the INT for the target channel is active; we have not observed this phenomenon since making this change.

 

B. Inconsistency between Character Timeout Indication and Data Ready States

During receive interrupt processing, we observed the following conditions:

 

IIR = 0xCC (Character Timeout Indication)

LSR = 0x60 (Data Ready = 0)

RXRDY for the target channel = Low (Active)

 

We understand that Character Timeout Indication and RXRDY indicate the presence of received data in the RX FIFO.

On the other hand, LSR’s Data Ready = 0 indicates that the RX FIFO is empty; therefore, the states of these signals and registers appear to be inconsistent.

In our implementation, we read the RBR only when Data Ready = 1.

Therefore, when this phenomenon occurs, we are unable to read the received data, and the interrupt handling may not complete normally.

 

[Similar Cases Confirmed on the TI E2E Forum, etc.]

Although we could not find any publicly reported cases specifically related to the TL16C2550, cases that are believed to be related have been reported for the following similar UART products.

 

■TL16C550D

A case where IIR = 0xCC and LSR = 0x60, preventing the receive interrupt from being processed normally

 

■TL16C752D

A case where, even after reading the RX FIFO, the state remains IIR = 0xCC, LSR = 0x60, and INT = Active

Additionally, cases have been reported where “0x03” is read from the IIR, a value that is difficult to interpret as a normal interrupt state.

 

■TL16C752B

Errata (SLLZ049) indicates that if the timing of an IIR read operation conflicts with the setting of the THRE Interrupt Condition, the THRE Interrupt Condition may be

unintentionally cleared.

Based on this information, we recognize that some TI UARTs have known issues related to the timing of internal interrupt state updates and register access.

 

[Questions]

1. Regarding the TL16C2550IPFB, are there any cases, known issues, or usage precautions that are the same as or similar to the two phenomena described above?

2. Is it possible that this is caused by internal circuitry or interrupt control logic shared with previous products such as the TL16C752B?

3. Please advise us of any known workarounds, recommended register access procedures, access intervals, etc.

4. We are also planning to adopt the TL16C752D for another product. Please confirm whether there are any similar known defects or issues with the TL16C752D.

If necessary, we can provide the acquired register values, bus access waveforms, and INT and RXRDY waveforms.

Best Regards,

ttd

  • Hi ttd,

    1. Regarding the TL16C2550IPFB, are there any cases, known issues, or usage precautions that are the same as or similar to the two phenomena described above?

    I haven't seen anything about phenomenon A, though I have seen phenomenon B. I am unsure of the reason the interrupt does not get cleared, but you can try resetting the RX FIFO by writing '1' to FCR bit 1, which should clear the interrupt.

    2. Is it possible that this is caused by internal circuitry or interrupt control logic shared with previous products such as the TL16C752B?

    Unfortunately I do not have much information on the older products, so I can't say for sure either way right now. I will try to look into this.

    3. Please advise us of any known workarounds, recommended register access procedures, access intervals, etc.

    See above answer to #1.

    We are also planning to adopt the TL16C752D for another product. Please confirm whether there are any similar known defects or issues with the TL16C752D.

    I am unaware of a similar defect with this product.

    -Ethan White

  • Hi Ethan White,

    Thank you for your answer.

    Please let me know if you find out anything about Q2.

    Best Regards,

    ttd

  • Hi Ethan White,

    We have conducted additional verification regarding this matter and are writing to inform you of the results and the items we would like you to re-verify.

    [Results of Additional Verification]

    Regarding the “inconsistency between Data Ready and the receive interrupt status” we previously reported, we observed the following conditions during transmission and reception tests using the return fixture:

    ・Receive Interrupt: Active

    ・IIR: 0xCC (Character Timeout Indication)

    ・LSR: 0x60 (Data Ready = 0)

    ・RXRDY: Low (Active)

    Normally, the RBR is not read when Data Ready = 0. However, when we read the RBR under the above conditions regardless of the Data Ready value, we were able to

    successfully retrieve the received data.

    Based on these results, we believe it is highly likely that, even though valid data actually exists in the RX FIFO, the LSR’s Data Ready is indicating 0.

    [Items to Be Reconfirmed]

    We apologize for the inconvenience, but could you please confirm the following with TI regarding the phenomenon described above?

    1. TI’s Recognition of the Phenomenon

    Regarding the phenomenon where “the LSR’s Data Ready indicates 0 even though valid data exists in the RX FIFO,” is this recognized by TI as a known defect or a known

    phenomenon?

    2. Existence of Errata and Known Issues

    Regarding the TL16C2550IPFB, are there any published or internal errata, known issues, or usage precautions related to the phenomenon described above?

    Additionally, if no errata have been issued at this time, please confirm whether there are plans to issue any in the future.

    3. Recommended Workaround

    Is the method you described—“writing a 1 to bit 1 of the FCR and resetting the RX FIFO”—an official workaround recommended by TI?

    I understand that resetting the RX FIFO erases any unread data within the FIFO. Therefore, please advise on any recommended procedures

    or alternative workarounds for processing received data without losing it.

    4. Applicability to the TL16C752D

    Our company plans to adopt the TL16C752D for another product. Regarding the TL16C752D, please confirm once again whether please reconfirm whether the phenomenon where “Data

    Ready becomes 0 even though data exists in the RX FIFO” is recognized as a known issue for the TL16C752D.

    Additionally, please let us know if there are any errata, known issues, or recommended workarounds for this product.

    If necessary, we can provide the register values, bus access waveforms, and observed waveforms for INT and RXRDY that we have captured.

    Best Regards,

    ttd

  • Regarding the phenomenon where “the LSR’s Data Ready indicates 0 even though valid data exists in the RX FIFO,” is this recognized by TI as a known defect or a known

    phenomenon?

    I'm not entirely sure what you are asking here. This has been seen in the past, if that answers your question.

    Regarding the TL16C2550IPFB, are there any published or internal errata, known issues, or usage precautions related to the phenomenon described above?

    Not that I am aware of.

    Is the method you described—“writing a 1 to bit 1 of the FCR and resetting the RX FIFO”—an official workaround recommended by TI?

    I understand that resetting the RX FIFO erases any unread data within the FIFO. Therefore, please advise on any recommended procedures

    or alternative workarounds for processing received data without losing it.

    I'm not exactly sure what constitutes an "official workaround". It is my understanding that the problem is that the interrupt is being triggered without any data actually being present in the RX FIFO, therefore clearing it to clear the interrupt should not be an issue.

    Our company plans to adopt the TL16C752D for another product. Regarding the TL16C752D, please confirm once again whether please reconfirm whether the phenomenon where “Data

    Ready becomes 0 even though data exists in the RX FIFO” is recognized as a known issue for the TL16C752D.

    Additionally, please let us know if there are any errata, known issues, or recommended workarounds for this product.

    Again, I am unaware of a similar defect with this product.

    -Ethan White

  • Hi Hi Ethan White,

    Regarding this matter, we have attached the following four documents used to verify the phenomenon.

    We provide the following supplementary information regarding the contents of each document.

    See attached files.

    Files for TL16C2550.zip

    [Attached Documents]

    ■ Diagram.png

    This document illustrates the configuration using the TL16C2550.

    The configuration converts PCIe access requests issued by the CPU into local bus access via the FPGA,

    and accesses two TL16C2550 devices.

    We are using two TL16C2550 devices, each configuring 2 channels, for a total of 4 UART channels.

    For each channel, we connected a fixture that loops the transmit signal back to the receive signal and conducted tests involving repeated transmission and reception.

    ■ 260813_iirCC8k_v2.ila

    This is the Vivado ILA data that served as the basis for “ScreenShot-260813_iirCC8k_v2.png,” described below.

    It can be viewed in Vivado 2023.2 or later.

    If necessary, we can also provide the data in CSV format.

    ■ ScreenShot-260813_iirCC8k_v2.png

    This is the ILA waveform captured when it was confirmed that the “Data Ready” state did not match the actual receive FIFO state.

    Below is a description of the main signals:

    ・adr_n_out[7:0]

    This signal combines device selection, Chip Select, and register address, and

    * bit[4]: Device selection

    * bit[3]: Chip Select selection

    * bit[2:0]: TL16C2550 register address

    ・data_in_0–3

    Since the CPU’s PCIe access is 32 bits wide, the read data is split into 8-bit segments for observation.

    The correspondence with the 32-bit data is as follows:

    [31:0] = {data_in_3[7:0], data_in_2[7:0], data_in_1[7:0], data_in_0[7:0]}

    .

    In this waveform, the relevant data_in_1 and data_in_2 signals are displayed.

    ・SIO_A(B)_RXRDY1(2)_N_IBUF

    This is the RXRDY output signal of the TL16C2550.

    On the waveform display, it corresponds to CH1, CH2, CH3, and CH4, in that order from top to bottom.

    In this waveform, the phenomenon is occurring on CH4.

    [Operation on the Waveform]

    At the trigger point (around 100 pt),

    adr_n_out = 0x1A,

    and it is reading the CH4 IIR (Register Address = 2).

    At this point,

    IIR = 0xCC

    is read from the TL16C2550, confirming that a Character Timeout Indication has occurred.

    Subsequently, at the yellow cursor position (around 2,061 pt),

    adr_n_out = 0x1D

    indicating that the LSR (Register Address = 5) of CH4 is being read.

    At this point,

    LSR = 0x60

    is read.

    Therefore,

    LSR[0] Data Ready = 0

    .

    Note that there are two write accesses near 1,000 pt;

    however, both are accesses to the IER (Register Address = 1)

    and do not directly affect the presence or absence of data in the receive FIFO being examined here.

    Furthermore, during this period, CH4’s RXRDY remains continuously Low (Active).

    Therefore, in this waveform,

    * IIR = 0xCC (Character Timeout Indication)

    * RXRDY = Low (Active)

    * LSR = 0x60 (Data Ready = 0)

    are observed simultaneously.

    ■ log_DataReady-Error_260903.txt

    This is the operation log acquired on the CPU side.

    It is a log recorded when a timeout occurred in the reception processing within the program during a test involving repeated transmission and reception.

    This event occurred on CH3 (/ttyS6), and when IIR, LSR, and RBR were read for debugging purposes at the time of the timeout,

    IIR = 0xCC

    LSR = 0x60

    RBR = 0x42

    were confirmed.

    In other words,

    * IIR indicates a Character Timeout

    * LSR indicates Data Ready = 0

    * However, when RBR is actually read, valid received data (0x42) can be successfully retrieved

    This is the state observed.

    Based on these results, we have determined that, at least at the time this issue occurred, valid data was present in the receive FIFO,

    yet only the LSR’s Data Ready was showing a value of 0.

    Furthermore, we have observed a similar phenomenon on CH4 in the ILA waveform and on CH3 in the CPU log,

    and therefore believe this is not a phenomenon limited to a specific UART channel.

    If there is any additional information required, or any signals, registers, etc., that need to be verified,
    we will obtain them to the extent possible, so we would appreciate it if you could contact us.

    Best Regards,

    ttd

  • Hi ttd,

    I saw your email, so thank you for the background info on this project. If it is ok with you, for now, I will keep responding on E2E to help anyone in the future with a similar problem.

    Just to clarify, is your concern here that resetting the FIFO to clear the interrupt will be potentially clearing valid data received?

    Have you tried resetting the RX FIFO in this setup and seeing if data is received normally after that? I notice that in your setup the RXRDY! pin is always low which would indicate that the RX FIFO is never empty. I would be interested to see if resetting the RX FIFO would change the test results.

    -Ethan White

  • Ethan White,

    I apologize for the late reply.

    I have reviewed the matter you requested.

    Could you please provide some advice?

    ■ Are you concerned that resetting the RX FIFO to clear an interrupt might also erase valid received data?

    That understanding is correct.

    As shown in the operation log I sent previously,

    ・IIR=0xCC

     ・LSR=0x60 (Data Ready = 0)

     ・RBR=0x42

     we confirmed that even when Data Ready is set to 0, valid received data actually remains in the RX FIFO.

     Therefore, we are concerned that resetting the RX FIFO in this state would also discard the valid received data.

    ■Can data still be received normally after resetting the RX FIFO?

     After verification, we confirmed that data could still be received normally even after the reset.

     We reset the RX FIFO after a timeout occurred and checked the status immediately afterward; the following conditions were observed:

     ・IIR=0xC1

     ・LSR=0x60

     ・RXRDY=High

     When we resumed transmission and reception from this state, we confirmed that subsequent received data was received normally.

    ■Additional notes regarding the ILA waveform we previously sent, specifically that RXRDY was consistently Low

     During the recording period of the waveform in question, we did not perform any operations to empty the RX FIFO, including resetting the RX FIFO or reading out received data.

     Therefore, we believe that RXRDY did not transition to High during the recording period.

    ■ Additional Information

     In situations where we determined that “Data Ready” did not match the actual state of the RX FIFO,

     we have confirmed that “Data Ready” may return to a normal state when new received data is stored in the RX FIFO and the FIFO is updated.

    Best Regards,

    ttd

  • Hi ttd,

    My suggestion here would be to possibly add a dummy read of the FIFO before you clear it by writing 1 to FCR. This would make sure you don't loose any data.

    -Ethan White

  • Hi Ethan White,

    I would like to confirm the method you proposed this time:

    “Read the RBR once before clearing the RX FIFO.”

    Please allow me to ask a few questions regarding this.

    Q1
    Is this the method recommended by TI as a workaround for this issue?

    Q2
    In that case, are we to treat the value read from the RBR as valid received data?

    Best Regards,

    ttd

  • Is this the method recommended by TI as a workaround for this issue?

    This is a potential solution I encourage you to test on your own system.

    In that case, are we to treat the value read from the RBR as valid received data?

    Based on your testing you found that when the timeout occurs there is valid data on the RBR, so yes.