This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXU0304-Q1: Slew rate during tPD definition

Part Number: TXU0304-Q1

Hello Expert,

 

How much slew rate did you used when you defined tPD?

In timing chart, tPD is delay from signal exceed to low/high against VCCI/2


On the other hands, this device's Vit is not VDDI/2 due to it have hysteresis and variation.
For example, Vit_neg during 1.1V is 0.31V~0.48V againt 0.55V=VDDI/2.

Then, tPD definition should be different if slew rate of input signal too slow.
Moreover, this device don't have any limitaion for slew rate of input signal.

Therefore, we'd like to now how much slew rate is anticipated during tPD definition.

image.png

 

Best regards,
Kazuki Kuramochi