This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25751A: Sleep Mode Current Consumption and CC Pin Wake-Up Functionality

Part Number: TPS25751A

Hi team,
I have a question regarding the current consumption in Sleep Mode.
According to the datasheet, the Sleep Mode current is specified as IVIN_3V3,Sleep = 56 µA.
  • Can we consider that the device consumes only 56 µA in Sleep Mode?
  • Does this current consumption include the circuitry required to keep the wake-up function active, such as monitoring the USB Type-C CC pins?
  • In other words, is the 56 µA current mainly consumed to maintain the wake-up detection capability while the device remains in Sleep Mode?
Best Regards,
 Shota