Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8044A: Device comparison

Part Number: TUSB8044A
Other Parts Discussed in Thread: TUSB8041A

Hi team,

In the comparison table below, I have some questions.

[Q1]

TUSB8044A has four "No" items.
What are the mean of these items?

  • HS connection indicator
  • SS connection indicator
  • HS suspend indicator
  • Multiple SMBus slaves address options

[Q2]

Regarding TUSB8044A, Can we configure following settings via Pin strap?

  • Inndividual / Gang
  • Power Switch ENABLE logic
  • Enable/Disable of BC1.2

 

Best regards,
Goto

  • Hi,

    [Q1]

    TUSB8044A has four "No" items.
    What are the mean of these items?

    • HS connection indicator
    • SS connection indicator
    • HS suspend indicator
    • Multiple SMBus slaves address options

    We can look at the TUSB8041A datasheet to see what these indicator pins do:

    The TUSB8041A indicators will function in either I2C or SMBus mode and SMBus Address is adjustable.

    The TUSB8044A indicators will only function in SMBus mode. In I2C mode these pins will serve billboard functionality. The SMBus address is also static in the TUSB8044A.

    Regarding TUSB8044A, Can we configure following settings via Pin strap?

    • Inndividual / Gang
    • Power Switch ENABLE logic
    • Enable/Disable of BC1.2

    Yes, all of these can be configured in pin-strap mode.