Part Number: TMDS1204
Other Parts Discussed in Thread: TDP1204
I am trying to output TMDS/FRL signals by applying an HDMI IP to an FPGA.
But due to the characteristics of the FPGA GT (GPIO out), it only supports a 0 to 800mV swing without a common-mode voltage.
However, it is my understanding that the standard signal for TMDS/FRL is a 500mV swing with a 3.3V common mode.
Therefore, I would like to use the TMDS1204 to convert the 0 to 800mV signal into a signal with a 3.3V common mode.
I am inquiring whether it can be used for this type of application.
Additionally, is there a specific part that needs to be configured via I2C when the TMDS1204 outputs TMDS or FRL?