Other Parts Discussed in Thread: SN65LVPE502CP
Hi,
I am Jing Li from MIssouri S&T. I have ordered USB 3.0 repeater SN65LVPE502CP EVM, is there anybody who can help me to find where its gerber file?
Since I only want the radiation or noise from the chip SN65LVPE502CP, but the signal traces from IC could also radiate a lot which I do not want, with gerber file probably I will try to modify some traces and run them immediately to the other side of the board, where the IC pins touch the pads.
Also I heard of that usually each IC will be performed EMI test before it manufactured, so if possible, could I have a TEM cell board of SN65LVPE502CP which is designed for EMI test?
Thanks a lot for your great help!
Thanks,
Jing