This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Differential driver picture

I posted a question about differential driver but looks like the picture didn't attach to the post.

Please see attached picture below for more details and referee back to the question about differential driver

  • Hi,

    Can anyone out there help me get a circuit that can do a differential amplifier input of two separate source and get the output of the input.

    Technically we're looking for a circuit that can take two different Ethernet connection from two separate sources and give out two separate output.

    Below is the ideally circuit design but I can't find one that can take two inputs at once special consider that it has to be Ethernet input and output.

    Regards,

    Bhegin

  • why don't you use two separate receiver circuit and logic OR-gate the receiver outputs?

    you probably can loock them against each other.

    regards, Thomas