Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLIN1028-Q1: Question about watchdog function

Part Number: TLIN1028-Q1
Other Parts Discussed in Thread: TLIN1431-Q1

Dear TI experts,

Do you have any ideas about making watchdog function using EN pin or nRST pin of TLIN1028-Q1?

(I.e. sending reset signal to host MCU if LIN communication is unavailable for the specific time duration)

Please check this issue. Thanks.

Best regards,

Chase

  • Hi Chase,

    Please note that the data sheet specifies that nRST is pulled low when the VCC undervoltage condition persists beyond the specified detection time, and it returns high when VCC recovers. Hence, it should not be related to LIN communication activity and may not be configured to go low if no LIN message is observed within a specified time.

    Furthermore, EN may be used to force the device into/out of sleep. However, there should be no internal timer that automatically changes EN when LIN communication stops.

    Hence, would recommend an external watchdog or a device with the feature (TLIN1431-Q1 for example) as needed, thanks.

    Best Regards,

    Michael.