Other Parts Discussed in Thread: DS90CR287
Hello,
I'm using this serializer to connect an image sensor to a Frame Grabber with the DS90CR287a receiver chip installed.
When probing the output LVDS pairs, I notice that the (+) line is averaging 1.6V and the (-) line is averaging 1.3V. This is on a regularly ocuring clock line. I am new to LVDS logic, but I thought the (-) line really had to be negative in voltage?
If so, that may be why I can't communicate with our Frame Grabber. In that case, I was still unclear as to a few things from the spec sheet.:
- Are the PLL_VCC, LVDS_VCC, and VCC all supposed to be tied to 3.3V?
- Are all grounds okay to be tied to the same ground plane?
- pin 32, the PWR_DWN line is suppoed to be 3.3V in normal operation, correct?