Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1146-Q1: Selective Wake-up from Standby mode

Part Number: TCAN1146-Q1

Hi Team,

In Standby Mode with selective wake-up enabled I need to send 2 frames; 1 to enable WUF receiver and 1 to actual wake-up.

What would happen if between these frames I send some SPI communication to SBC? Does this affect the WUF receiver.

From my tests it seems that it does. I have 2 scenarios:

  1. I send 2 WUP frames at a distance of 50milliseconds; SBC wake-up
  2. I send 1 WUP frame, I send an SPI command(check status), I send another WUP frame; SBC does not wake up.

Could you confirm this?

Thanks,

Cornel

  • Hi Cornel,

    SPI is a different IP than the selective wakeup receiver, it should not affect each other. What SPI command did you send? i.e which register did you configure? 

    Also, what's the time slot between two WUFs in scenario 2?

    Regards,

    Sean