Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90CR288A: Similar product search

Part Number: DS90CR288A
Other Parts Discussed in Thread: DS90CF386


I required a receiver converts the four LVDS data streams back into 28 bits of LVCMOS/LVTTL data similar to DS90CR288A. I need to connect the output to a 1.8V bank. As DS90CR288A only works in 3.3V, suggest any similar product with transmit clock frequency not leaa than 80 MHz and whose output i can directly map to 1.8v bank

  • Hello Neeraj,

    I have tried to find a match for your 28-bit, 80 MHz, and 1.8V output criteria. Based on the available specifications, the DS90CF386 is the closest match regarding your frequency requirement. It supports a clock range of 20 MHz to 85 MHz, which meets your need for a clock rate of at least 80 MHz. However, it is important to note that the DS90CF386 is designed for a 3.3V supply.

    Currently, we do not offer a direct functional equivalent to the DS90CR288A that features native 1.8V output levels for the LVCMOS/LVTTL bank. If you must interface with a 1.8V bank, you may need to consider using a level translator or a voltage-level shifter between the receiver output and your target device. 

  • Hi,

    Thank you for the reply.

    As a thought, isn't it essential to have a similar IC, given that native 3.3V banks are declining in modern FPGAs?

    And as you mentioned, when a 3.3V LVCMOS output is level translated and mapped to a 1.8V FPGA bank, is there a potential risk of added noise, delay, or other signal integrity issues?

    If using a level shifter is the best approach, which specific ICs would you recommend as the best solution for this use case? 

  • Hi,

    Please refer to this App not where a similar approach is described.

    How to Support 1.8-V Signals Using a 3.3-V LVDS Driver/Receiver + Level-Shifter