TMUXHS4612: TMUXHS4612: Can I use this MUX for single ended (eMMC & MicroSD Card) interface!

Part Number: TMUXHS4612

Hi,

I am using a Differential 1:2 MUX (TMUXHS4612IRETT) to switch between the single-ended eMMC and MicroSD card interfaces.

All single-ended signals operate at 1.8 V. The common port of the MUX is connected to the Agilex-9 HPS (1.8 V), with the normally closed (NC) port connected to eMMC (1.8 V) and the normally open (NO) port connected to MicroSD (3.3 V) through a level shifter.

Kindly confirm whether this Differential 1:2 MUX can be used for this application, where all signals are single-ended. The maximum clock frequency for both interfaces is 50 MHz.

Please refer to the attached schemtic of the same.

SCHEMATIC1 _ PAGE1.pdf 

Best Regards,
Raj