This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD4431A: co-layout XR34350

Part Number: THVD4431A
Other Parts Discussed in Thread: THVD4431,

Hi

If the customer is currently using the XR34350 and wants to co-layout the THVD4431 for evaluation, where in the schematic diagram does it need to be adjusted?

Thanks

  • HI Gareth,

    The only difference between the the THVD4431A and XR34350's pinouts would be Pin 13. XR34350 has that as a NC, while the THVD4431A has that as MODE2 which toggles loopback mode. If your customer does not need loopback mode then they are ok to leave Pin 13 as a NC for the THVD4431A as there is an internal pull down.

    -Ethan White