Part Number: DP83825I
Hi,
In our application, DP83825IRMQR, we are driving an LED(green, VF=2.0V) using the LED0 (pin 4) to indicate Activity and Link status. There are 2 questions.
No.1)What is the maximum drive strength of this pin? (ex. Iout of LED0=5mAtyp.~10mAmax. etc.)
No.2)Can it safely drive an LED with a 10mA* source current? (*considering the IF[mA] of LED and 1.3mA for "auto neg")
Thanks,
Tommy