Part Number: TMDS181
Bits [7:2] can be written and read back correctly, but bit[1:0] always read back 0, write has no effect.
I2C_EN pin is pulled HIGH (I2C register mode).
My application: FPGA -> TMDS181 -> HDMI RX, 4K60 Retimer mode.
Part Number: TMDS181
Bits [7:2] can be written and read back correctly, but bit[1:0] always read back 0, write has no effect.
I2C_EN pin is pulled HIGH (I2C register mode).
My application: FPGA -> TMDS181 -> HDMI RX, 4K60 Retimer mode.
Hi,
Is the TMDS181 HPD_SNK high in this case?
Thanks
David