Part Number: TCAN4551-Q1
Other Parts Discussed in Thread: TCAN4572-Q1, TCAN4550, TCAN4550-Q1
Dear TI experts,
My customer is looking for a CAN controller with integrated transceiver.
I think TI has only 2 devices ; TCAN4551-Q1 and TCAN4572-Q1.
The concern is that the range of Vsup is nominal 5.6V, maximum 5.9V.
In the case of startup, Vsup would be lower under 5.5V. It is out of recommended rage of TCAN4551-Q1.
(The recommended range of Vsup is 5.5V ~ 30V in the datasheet.)
- Can TCAN4551-Q1 operate normally under the condition of Vsup=5.6V condition? (Startup and CAN/CAN FD operation)
- Is there any possibility of going to startup failure or reset or shutdown status if Vsup voltage is going to under 5.5V during startup or operation?
- Is it okay to use Vsup=5.9V maximum by buck converter or other power devices?
- Do you think it is okay to use Vsup=5.6V nominal and 5.9V maximum conditions?
- Should I consider more about the parameters Vsup startup rising time, undervoltage Vsup threshold, power-on reset and voltage drop situation if my customer use Vsup=5.6V nominal and 5.9V maximum conditions??
- Doyou think it is better to use TCAN4572-Q1 than TCAN4551-Q1? (Its range of Vsup is wider than TCAN4551-Q1, 4.5V~36V)
Best regards,
Chase