Part Number: TCAN1044A-Q1
Hello,
I am designing a CAN interface using the TCAN1044A-Q1 and I would like to ask for your recommendation regarding the PCB trace impedance.
My PCB stack-up makes it difficult to achieve a 120 ohm differential impedance without using very narrow traces. The relevant geometry is:
-
Internal CANH/CANL differential pair
-
Trace width: 0.10 mm
-
Differential spacing: 0.34 mm
-
Copper thickness: 18 µm
-
H1 to the GND reference plane: 0.10 mm
-
H2 to the adjacent layer: 0.36 mm
-
Dielectric Dk: approximately 4.45 @ 100 MHz
With this geometry, my field-solver calculation gives approximately 100 ohm differential impedance, compared with the nominal 120 ohm CAN bus impedance, so there is approximately a 17–20% impedance deviation.
The CANH/CANL routing from the TCAN1044A-Q1 to the CAN connector is approximately 90 mm.
This limitation is caused by the fact that the same PCB stack-up is also being used for high-speed USB and Ethernet interfaces, which impose specific controlled-impedance requirements that must be met. Therefore, the available trace geometry for the CAN differential pair is constrained by the overall PCB stack-up and the impedance requirements of these other interfaces.
My main question is:
Would a 100 ohm differential PCB impedance, rather than 120 ohm, be a significant concern for a 90 mm CANH/CANL connection to the TCAN1044A-Q1?
I am particularly interested in whether the 20% impedance deviation is likely to cause a meaningful signal-integrity issue for this PCB trace length, or whether the relatively short 90 mm section can reasonably be treated as a small impedance discontinuity compared with the 120 ohm CAN cable.
If 120 ohm should be considered necessary in this case, could you recommend how you would approach this problem? I would prefer to avoid reducing the trace width further because the transceiver has a 130 mA bus-fault current, and I would like to maintain adequate PCB trace robustness.
Thank you in advance for your advice.