Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: Issue with MCU SPI in peripheral mode

Part Number: AM6442
Other Parts Discussed in Thread: TMDS64EVM, SYSCONFIG

I am facing issue with MCU SPI in peripheral mode.

AM6442 (AM64x family) (TMDS64EVM) MCU_M4FSS0_CORE0 (M4F)

Interface: MCU_SPI0 (clock phase and polarity mode 3), peripheral (slave) mode, 3-pin configuration, 8 bit data.

Connector: Safety J1

Pin 16 → MCU_SPI0_CLK (external clock input)

Pin 4 → MCU_SPI0_D0 (MISO output)

Pin 2 → MCU_SPI0_D1 (MOSI input)

Pin 23 → DGND (common ground)

I am proving external clock with common ground.

Problem:

TX transmits independently of clock, clock behaves as a chip-enable signal rather than clock: TX Data Not Synchronized with SPICLK.

Debugging:

M4F writes 0x99 (any data) to MCSPI_TX0 when CH0CTRL.EN=1

Data appears on MISO (D0) but does NOT shift synchronously with SPICLK edges

Byte appears to transmit regardless of clock timing

Clock Input Acts as Enable, Not Clock

 

External SPICLK transitions do not generate SPI bit shifts

TX transmission continues without clock gating

Data timing independent of SPICLK level