LMH0397: Troubleshooting Video Flickering with LMH0397 in Equalizer Mode

Part Number: LMH0397

Dear Team,

We are currently utilizing the LMH0397 3G-SDI Equalizer/Cable Driver IC in our hardware design and are encountering a video flickering issue under specific operating conditions. We would appreciate your technical guidance in resolving this problem.

Observed Behavior & Test Results:

  • Equalizer Mode (Issue): When the IC is configured in Equalizer mode, we experience persistent video flickering and signal instability when connected to external 3G-SDI sources. This behavior is consistent across multiple sources, including a Blackmagic Design bidirectional HDMI-to-3G-SDI converter and a standard 3G-SDI camera.

  • Loopback Mode (Control): To isolate the signal path, we performed a loopback test using one channel as a cable driver and another as an equalizer, connected externally via a Belden 1694A cable. In this configuration, the output functions correctly without any flickering.

Given that the internal loopback test passes successfully, could you help us eliminate this flickering issue?