SN65LVDS391: TI part numbers component grade requirement

Part Number: SN65LVDS391

Dear Team,

Please Share Component grade (military, automotive, industrial, Commercial) for below mentioned TI part numbers.

1. SN65LVDS391PW
2. SN74ALVC245PWR
3. SN74LVC2G07DBVR / SN74LVC2G07DBVRG4
4. SN74LVC2G07DCKR
5. TPS7A8500RGRT

  • Hi Shenbagavalli,

    TI doesn't strictly distinguish between industrial and commercial grade parts in our rating system. You can see here for explanation of the system we use: https://www.ti.com/quality-reliability/certifications-standards/part-ratings.html

    That said, usually temperature range is the major distinguishing factor between commercial and industrial, so these would all be considered industrial grade with the following temp ranges: 

    1. SN65LVDS391PW (-40 to 85C) 
    2. SN74ALVC245PWR (-40 to 85C)
    3. SN74LVC2G07DBVR / SN74LVC2G07DBVRG4 (-40 to 125C) 
    4. SN74LVC2G07DCKR (-40 to 125C) 
    5. TPS7A8500RGRT (-40 to 125C)

    Parts which are automotive grade from TI will typically have a Q near the end of their orderable part number (this is the part number you see with packaging information, in the "Ordering and Quality" section of the parts page on ti.com, ex. TCAN1145DMTRQ1), they will also have a "-Q1" suffix on the general part number itself (ex. TCAN1145-Q1). 

    Best Regards,
    Brandon Fisher