Part Number: TUSB522P
Hello TI Team,
The attachment is the schematic of TUSB522PIRGER.
Could you have a check?
TUSB522PIRGER_Schematic_20261006.pdf
Best Regards!
Wang Jingkun
Part Number: TUSB522P
Hello TI Team,
The attachment is the schematic of TUSB522PIRGER.
Could you have a check?
TUSB522PIRGER_Schematic_20261006.pdf
Best Regards!
Wang Jingkun
Hi,
Here is the schematic review: TUSB522p_Schematic_Review_Faurecia_NA_NA (10_6_2026).pdf
Hi,
Add some comments on this document, could you check it again?
TUSB522p_Schematic_Review_Faurecia_NA_NA (10_6_2026)_Reply.xlsx
Best Regards
Hi,
Pins 8,9: OK
Pin 11,12: OK
Pins 22,23: ESD diodes implemented. Please ensure that the clamping voltage of the ESD diodes does not exceed the abs. max voltage rating of the pins of TUSB522p. Recommended implementation is to have a 0201 0-ohm series resistor between the TUSB522p and ESD diode for ESD tuning.
Pins 19,29: ESD diodes implemented. Please ensure that the clamping voltage of the ESD diodes does not exceed the abs. max voltage rating of the pins of TUSB522p. Recommended implementation is to have a 0201 0-ohm series resistor between the TUSB522p and ESD diode for ESD tuning. AC coupling these pins is optional. I recommend these optional capacitors as it may improve interoperability. The AC coupling on these pins should be 330nF.
Hi,
Pins 19,20:
AC coupling these pins is optional. I recommend these optional capacitors as it may improve interoperability. The AC coupling on these pins should be 330nF.
Question:
Best Regards!
Wang
Hi,
Could you please clarify the statement, "The AC coupling on these pins should be 330 nF"? Does this requirement apply only to Pins 19 and 20, or should the AC coupling capacitors on all differential pins (8, 9, 11, 12, 19, 20, 22, and 23) be changed to 330 nF?
This comment only applies to pins 19, 20.