This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8044: TUSB8044AIRGCR eye diagram testing method and command under Linux

Part Number: TUSB8044

Hi sir, 

Do you have TUSB8044AIRGCR eye diagram testing method and command under Linux?

Thanks a lot!

  • HI,

    You can try the following command:

    /* Send Endpoint Reflector control transfer */

    int ret = libusb_control_transfer(handle, bmRequestType, bRequest, wValue, wIndex, NULL, 0, 5000);

    // for usb2
    uint8_t bmRequestType = 0x23;
    uint8_t bRequest = 0x03;// set feature
    uint16_t wValue = 0x0015;
    uint16_t wIndex = 0x040x;// 4 is test package. x is port
    unsigned char *data = 0;
    uint16_t wLength = 0x0000;
    unsigned int timeout_ = 50000000;


    // for usb3
    uint8_t bmRequestType = 0x23;
    uint8_t bRequest = 0x03;// set feature
    uint16_t wValue = 0x0005;
    uint16_t wIndex = 0x0A0x;// x is port number
    unsigned char *data = 0;
    uint16_t wLength = 0x0000;
    unsigned int timeout_ = 50000000;