Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90LV019: Thermal Information for DS90LV019

Part Number: DS90LV019
Other Parts Discussed in Thread: DS90LV049

Required thermal information for the component DS90LV019,
Junction temperature
Operating temperature range
Thermal resistance value from Junction-to-ambient
thermal resistance value from Junction-to-case (top)
thermal resistance value from Junction-to-board

  • Hi Sharath,

    Junction temperature

    There is no specified maximum junction temperature for this device, this is pretty common with older devices like this. My general guidance for junction temperature would be to try to keep the device within the 85C recommended operating range and otherwise within its absolute maximum ratings and it should be fine. 

    That said, we have qualification data for this part up to 125C at 1000 Hours, and the storage temp is up to 150C, which some people take as the maximum junction temperature on these older parts that don't have them specified ( SN65LVDS389: Maximum Operating Junction Temperature of SN65LVDS389DBT ), We've also got other devices in this same family, released in the same timeframe such as DS90LV049 that list 150C maximum junction temperature. I would recommend taking the more conservative 125C upper bound. 

    Operating temperature range

    The Recommended Operating Temperature range is -40 to 85C.

    Thermal resistance value from Junction-to-ambient
    thermal resistance value from Junction-to-case (top)
    thermal resistance value from Junction-to-board

    What package do you want the thermal resistance values for? I can check if we have them internally or request them from our modeling team otherwise.

    Best Regards,
    Brandon Fisher