Other Parts Discussed in Thread: DS30BA101, DS30EA101, DS15EA101, DS15BA101, DS32ELX0124, DS32EL0421, DS32EL0124, DS32ELX0421
Hello All,
I was looking at using the DS30BA101 Cable driver and corresponding DS30EA101 cable equalizer in a system I am designing. In the datasheet on page 7, it shows a configuration with these chips using a 75 ohm unbalanced co-ax transmission line. Here is the question I have, instead of driving a 75 ohm load, can this device drive a 50 ohm unbalanced co-ax cable? Can this part do that by simply changing the resistor configurations to be 50ohm/25Ohm values? For my application, I can't use a 75Ohm coax connector due to constraints, and 50 ohm is required.
These parts seem very similar to the DS15BA101/DS15EA101 chip pair, but I need to go up to 3.125Gb/s. If this chip pair can't do it, are their other chips that TI has that can drive an unbalanced 50 ohm co-ax from DC upto 3.125Gb/s?
Thanks for any help.
Jesse C.