Part Number: TPS25751A
Hi team,
I have a question regarding the GPIO event configuration described in the TPS25751A TRM.
For example, if I want to assign Event 3, "Cable_Orientation_Event," to the GPIO 0 pin, should I convert the Event number "3" to binary and configure the corresponding bits as shown below?
| bit | 295 | 294 | 293 | 292 | 291 | 290 | 289 | 288 |
|
Set Value |
0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 |
In other words, is my understanding of the bit assignment for selecting Event 3 on GPIO 0 correct?
Best Regards,
Shota