SN75DP149: Suggestions for DP to DVI

Part Number: SN75DP149

Hello,

I am working on a PCB that will take DP++ input from a PC104 computer and convert the signals to DVI so it can be connected to a DVI input only monitor.  I have 5V available on the PCB but can geenrate 3.3 if needed.  What ICs are recommended? WHat are some things to consider when selecting a suitable IC? Thank you!