TPS25751A: Applicability of the TPS25751 EC Patch-Bundle Loading Procedure to TPS25751A

Part Number: TPS25751A
Other Parts Discussed in Thread: TPS25751,

Hi team,
 
The following application note describes how an embedded controller (EC) loads a patch bundle directly to the TPS25751:
 
Can the same procedure, including the I2Ct interface, Patch Burst Mode (PBM), 4CC commands, and the transition from PTCH mode to APP mode, be applied to the TPS25751A without any changes?
 
If there are any differences or additional requirements for the TPS25751A, please clarify them.
 
Best Regards,
Shota