TCA9517: Schematic review

Part Number: TCA9517

Hi team,

Would you please review below schematic? thanks!

  • P3V3 is a 3.3V bias voltage supplied on-board.

  • P5V_In is a 5.0V input rail supplied by the camera.

  • VCC_5V0_IN is a 5.0V bias voltage supplied on-board.

The A-side is connected to the connector I2C, while the B-side is connected to the CPU's I2C interface.

  1. Could you please confirm if the bias voltages connected to VCCa and VCCb are correct?

  2. Are the pin connections for SCLa/SDAa and SCLb/SDAb hooked up properly?