Part Number: TL16C2550
Hi team,
I have the following questions regarding the transmit and receive operations of the TL16C2550IPFB.
Transmit operation
- After starting data transmission from TXA, is it necessary to keep CSA Low until the transmission is complete?
- Is the CPU notified of transmission completion through an INTA interrupt?
Receive operation
- When data is received through TXA/RXA, is the CPU notified of reception completion through an INTA interrupt?
- Does this mean that the CPU does not need to continuously wait for incoming data and can read the receive buffer after the interrupt occurs?
Best Regards,
Shota