Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

DS100BR111: DS100BR111SQE SI Simulation Inquiry

Part Number: DS100BR111
Other Parts Discussed in Thread: DS110DF111

Hi 

  1. Regarding our current SI simulation topology for the DS100BR111SQE (shown in the diagram below) and IBIS mode is "snlm276", the current trace length configuration is as follows. Could you please check if this setup is acceptable? Thanks.ced34a56-5905-4552-ab1f-60d17033a792.png
  2. Our current simulation yields two different results. Which one should we rely on as the standard?Thanks.(1) Full-topology simulation: This covers the entire topology but results in a MAC RX failure (see the figure below) 

d2545bc5-e6f2-49ca-a346-a6e2364dfe79.png

 

(2) Segmented simulation: When we simulate the topology in separate segments, the results pass.

image.png

 

  • Hi

    Friendly reminder on this request.

  • Hi Vince,

    1. I would recommend reviewing SFF-8431 specification.  It has a recommended host channel insertion loss.  You should ensure your loss between redriver and SFP port meet this.

    2. I would recommend following the simulation topology recommended in the example project in snlm276.

    3. One additional way you can de-risk your design is by adding by adding a few placeholders to support the DS110DF111 retimer device.  This device uses same footprint as DS100BR111, and most of the pins are the same.  In case DS100BR111 jitter performance is not sufficient, DS110DF111 would improve jitter.

    Provisions:

    • Add provision for 25 MHz clock (REFCLK_IN)
    • Add provision for 22nF capacitor between LPF_CP_x / LPF_REF_x pins.

    DS100BR111

    DS110DF111

    Thanks,

    Drew