Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

TLK1211: TLK1201 Replacement

Part Number: TLK1211

Hi, 
I want to ask about TLK1201 and TLK1211.
Is TLK1211 the successor or replacement for TLK1201?
dear
  • Hi Takada-san,

    It looks like the TLK1211 would be a good replacement for the TLK1201.  It's pin to pin compatible and looking over the data sheet, it appears to be almost identical.  One difference that I noticed is that the TLK1201 seems to be designed for transmission over 50 Ohm or 75 Ohm media, while the TLK1211 is targeted towards just 50 Ohm.  Beyond this, the differences between the devices seemed to be limited to some variation in the electrical characteristics of the devices.  The TLK1211 does draw a bit more power, so it would be important to ensure that the system has appropriate margin for this.  I would recommend comparing electrical characteristics to ensure there are no surprises.

    Thanks,

    Drew