P82B715: Sx/Sy Input Current Requirement

Part Number: P82B715
Other Parts Discussed in Thread: TCA9617B

Hi team,

Background

We are considering connecting an MCU I2C port directly to the Sx/Sy pins of the P82B715.
The datasheet shows an internal 30-ohm sense resistor, but we could not find the current threshold required to activate the internal pull-down circuit.

Questions

  1. What is the current threshold at Sx/Sy to activate the internal pull-down circuit?
  2. Is a min/max value available, including process and temperature variations?
  3. If the threshold is not specified, is 3 mA sink capability at Sx/Sy an appropriate design requirement for the MCU?

Best Regards,
Ryu.